public interface DriveScrewNotOKParameters
This interface provides parameters relevant for generating script code for the Drive Screw Not OK feedback capability
(registered using ScrewdriverFeedbackCapabilities.registerDriveScrewNotOKCapability(ScriptCodeGenerator)
).
These parameters are passed when PolyScope calls the implementation of the ScriptCodeGenerator.generateScript(ScriptWriter, Object)
method responsible for the generating the script code.
Copyright © 2023. All rights reserved.