public static enum CommunicationInterfaceConfig.StopBits extends Enum<CommunicationInterfaceConfig.StopBits>
Modifier and Type | Method and Description |
---|---|
static CommunicationInterfaceConfig.StopBits |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static CommunicationInterfaceConfig.StopBits[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final CommunicationInterfaceConfig.StopBits ONE
public static final CommunicationInterfaceConfig.StopBits TWO
public static CommunicationInterfaceConfig.StopBits[] values()
for (CommunicationInterfaceConfig.StopBits c : CommunicationInterfaceConfig.StopBits.values()) System.out.println(c);
public static CommunicationInterfaceConfig.StopBits valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2023. All rights reserved.