Interface | Description |
---|---|
UserInteraction |
This interface provides functionality for requesting input or actions from end users
|
Class | Description |
---|---|
RobotPositionCallback | Deprecated
Use
RobotPositionCallback2 instead. |
RobotPositionCallback2 |
The robot position callback based on
PositionParameters which composes several parameters defining a position
of the robot. |
Copyright © 2023. All rights reserved.