public interface Rotation
| Modifier and Type | Method and Description | 
|---|---|
| boolean | epsilonEquals(Rotation other,
             double epsilon,
             Angle.Unit unit)
 Indicates whether some other  Rotationobject is "approximately equal" to this one. | 
| boolean | equals(Object obj)Indicates whether some other  Rotationobject is "equal to" this one. | 
| double | getRX()Deprecated. 
 Use  getRX(Angle.Unit)instead. | 
| double | getRX(Angle.Unit unit)Provides the value of the Rx parameter in specified units. | 
| double | getRY()Deprecated. 
 Use  getRY(Angle.Unit)instead. | 
| double | getRY(Angle.Unit unit)Provides the Ry parameter value in specified units. | 
| double | getRZ()Deprecated. 
 Use  getRZ(Angle.Unit)instead. | 
| double | getRZ(Angle.Unit unit)Provides the Rz parameter value in specified units. | 
| int | hashCode() | 
| String | toString() | 
@Deprecated double getRX()
getRX(Angle.Unit) instead.@Deprecated double getRY()
getRY(Angle.Unit) instead.@Deprecated double getRZ()
getRZ(Angle.Unit) instead.double getRX(Angle.Unit unit)
unit - The angular unit for which to return the Rx parameterdouble getRY(Angle.Unit unit)
unit - The angular unit for which to return the Ry parameterdouble getRZ(Angle.Unit unit)
unit - The angular unit for which to return the Rz parameterboolean epsilonEquals(Rotation other, double epsilon, Angle.Unit unit)
 Indicates whether some other Rotation object is "approximately equal" to this one.
 
other - Another Rotation object.epsilon - The tolerance value to be used for the comparison of rotation parameters (i.e. Rx, Ry, Rz) in
                specified unitsunit - The angular unit for the specified epsilon tolerance.true if the values of this object is "approximately equal" to the values of the other
         argument; false otherwise.boolean equals(Object obj)
Rotation object is "equal to" this one.int hashCode()
Copyright © 2023. All rights reserved.