public interface Pressure
This interface represents pressure values.
The pressure values can be created using theSimpleValueFactory interface.| Modifier and Type | Interface and Description | 
|---|---|
| static class  | Pressure.Unit | 
| Modifier and Type | Method and Description | 
|---|---|
| boolean | equals(Object obj)Indicates whether some other  Pressureobject is "equal to" this one. | 
| double | getAs(Pressure.Unit unit)Provides the value in specified units. | 
| int | hashCode() | 
| String | toString() | 
double getAs(Pressure.Unit unit)
unit - the unit type.double value in the specified unit.int hashCode()
boolean equals(Object obj)
Pressure object is "equal to" this one.Copyright © 2023. All rights reserved.