@ProviderType
public interface PayloadContributionModel
This interface provides functionality for adding, updating and removing payloads in PolyScope.
Note: This interface must only be used in an installation contribution.Modifier and Type | Method and Description |
---|---|
Payload |
addPayload(String idKey,
String suggestedName,
Mass mass,
Position centerOfGravity)
Add a payload to the current installation in PolyScope.
|
Payload |
addPayload(String idKey,
String suggestedName,
Mass mass,
Position centerOfGravity,
InertiaMatrix inertiaMatrix)
Add a payload to the current installation in PolyScope.
|
InertiaMatrix |
createInertiaMatrix(double ixx,
double iyy,
double izz,
double ixy,
double ixz,
double iyz,
MomentOfInertia.Unit unit)
Creates an inertia matrix to be used when adding a payload to the installation in PolyScope using the method
addPayload(String, String, Mass, Position, InertiaMatrix) , or updating an existing payload using
updatePayload(String, Mass, Position, InertiaMatrix) . |
Payload |
getPayload(String idKey)
Returns the payload previously added by this URCap using the same
idKey identifier. |
void |
removePayload(String idKey)
Remove a payload added by this URCap from PolyScope.
|
void |
updatePayload(String idKey,
Mass mass,
Position centerOfGravity)
Update the mass and center of gravity (CoG) of an existing payload added by this URCap.
|
void |
updatePayload(String idKey,
Mass mass,
Position centerOfGravity,
InertiaMatrix inertiaMatrix)
Update the mass, center of gravity (CoG) and inertia matrix of an existing payload added by this URCap.
|
InertiaMatrix createInertiaMatrix(double ixx, double iyy, double izz, double ixy, double ixz, double iyz, MomentOfInertia.Unit unit)
Creates an inertia matrix to be used when adding a payload to the installation in PolyScope using the method
addPayload(String, String, Mass, Position, InertiaMatrix)
, or updating an existing payload using
updatePayload(String, Mass, Position, InertiaMatrix)
.
The inertia matrix is defined in a coordinate system with center at the payload's center of gravity (CoG), also referred to as center of mass, and the axes aligned with the tool output flange coordinate system (axes). The center of gravity is defined as the offset between the center of the tool output flange and the center of gravity of the attached payload.
The inertia matrix is specified by the six component values for the moments of inertia (i.e. Ixx, Iyy, Izz) and products of inertia (i.e. Ixy, Ixz, Iyz).ixx
- The moment of inertia around the x-axis. Must be positive.iyy
- The moment of inertia around the y-axis. Must be positive.izz
- The moment of inertia around the z-axis. Must be positive.ixy
- The product of inertia around the x and y axesixz
- The product of inertia around the x and z axesiyz
- The product of inertia around the y and z axesunit
- The unit for all the specified valuesPayload addPayload(String idKey, String suggestedName, Mass mass, Position centerOfGravity)
Add a payload to the current installation in PolyScope.
This makes the payload selectable by the end user as well as available to other URCap contributions (through the
PayloadModel
interface). The payload is not modifiable by the end user or other URCaps.
A default guess for the inertia matrix for the payload will be computed based on the specified payload mass and
center of gravity. If data for the payload's inertia matrix is available, the method
addPayload(String, String, Mass, Position, InertiaMatrix)
can used instead (this might give better
performance of the robot arm).
Note: The specified payload mass must be the total mass of the payload attached to the tool output flange of the robot.
The valid range for the payload mass and the coordinates of the center of gravity (CoG) are available through theRobotLimits
interface which can be accessed with RobotModel.getRobotLimits()
(an instance of the
RobotModel
interface can be retrieved through SystemAPI.getRobotModel()
).idKey
- The key to identify this payload by, not null
nor an empty string. The key is for this URCap
only, i.e. it only has to be unique for this URCap and not "globally" for other URCaps.suggestedName
- Suggested name for the payload, not null
nor an empty string. Valid names must match
regex [a-zA-Z][a-zA-Z0-9_]{0,14} for a total of 15 characters. The final name can be retrieved
from the returned payload instance.mass
- The total mass of the payload attached to the tool output flange of the robot, not null
. Create
it using SimpleValueFactory.createMass(double, Mass.Unit)
.centerOfGravity
- The center of gravity (CoG), also referred to as center of mass, for the payload. It is
defined as the offset between the center of the tool output flange and the center of gravity
of the attached payload. Cannot be null
. Create it using the PositionFactory
interface.PayloadAlreadyAddedException
- If a payload has previously been added using the same idKey
identifier.
Use getPayload(String)
to check if the payload has already been
added to the current installation.
Use updatePayload(String, Mass, Position)
or
updatePayload(String, Mass, Position, InertiaMatrix)
to update the
payload if the payload parameters have changed.IllegalPayloadNameException
- If the suggested name does not match required regex.IllegalMassException
- If the specified mass is not inside the valid range as defined by PolyScope.IllegalCenterOfGravityException
- If any of the values of the specified center of gravity are not inside
the valid range as defined by PolyScope.Payload addPayload(String idKey, String suggestedName, Mass mass, Position centerOfGravity, InertiaMatrix inertiaMatrix)
Add a payload to the current installation in PolyScope.
This makes the payload selectable by the end user as well as available to other URCap contributions (through the
PayloadModel
interface). The payload is not modifiable by the end user or other URCaps.
addPayload(String, String, Mass, Position, InertiaMatrix)
method instead if data for the
payload's inertia matrix is not available.
Note: The specified payload mass must be the total mass of the payload attached to the tool output flange of the robot.
The valid range for the payload mass and the coordinates of the center of gravity (CoG) are available through theRobotLimits
interface which can be accessed with RobotModel.getRobotLimits()
(an instance of the
RobotModel
interface can be retrieved through SystemAPI.getRobotModel()
).idKey
- The key to identify this payload by, not null
nor an empty string. The key is for this URCap
only, i.e. it only has to be unique for this URCap and not "globally" for other URCaps.suggestedName
- Suggested name for the payload, not null
nor an empty string. Valid names must match
regex [a-zA-Z][a-zA-Z0-9_]{0,14} for a total of 15 characters. The final name can be retrieved
from the returned payload instance.mass
- The total mass of the payload attached to the tool output flange of the robot, not null
. Create
it using SimpleValueFactory.createMass(double, Mass.Unit)
.centerOfGravity
- The center of gravity (CoG), also referred to as center of mass, for the payload. It is
defined as the offset between the center of the tool output flange and the center of gravity
of the attached payload. Cannot be null
. Create it using the PositionFactory
interface.inertiaMatrix
- The inertia matrix of the payload, defined in a coordinate system with center at the payload's
center of gravity and the axes aligned with the tool output flange coordinate system (axes).
Cannot be null
. Create it using
createInertiaMatrix(double, double, double, double, double, double, MomentOfInertia.Unit)
.PayloadAlreadyAddedException
- If a payload has previously been added using the same idKey
identifier.
Use getPayload(String)
to check if the payload has already been added to
the current installation.
Use updatePayload(String, Mass, Position)
or
updatePayload(String, Mass, Position, InertiaMatrix)
to update
the payload if the payload parameters have changed.IllegalPayloadNameException
- If the suggested name does not match required regex.IllegalMassException
- If the specified mass is not inside the valid range as defined by PolyScope.IllegalCenterOfGravityException
- If any of the values of the specified center of gravity are not inside
the valid range as defined by PolyScope.IllegalInertiaMatrixException
- If any of the values of the specified inertia matrix are not inside the
valid range as defined by PolyScope.Payload getPayload(String idKey)
idKey
identifier. Use this to verify if
the payload is present in the current installation.idKey
- The key to identify this payload by, not null
nor an empty string.null
if no payload exists in current installation (with the specified idKey
identifier).void updatePayload(String idKey, Mass mass, Position centerOfGravity)
Update the mass and center of gravity (CoG) of an existing payload added by this URCap.
Note: If an inertia matrix has been specified for the payload, calling this method will replace (overwrite) it with a computed default guess based the new specified payload mass and center of gravity. To avoid overwriting an existing inertia matrix (or to update an existing inertia matrix), instead use the methodupdatePayload(String, Mass, Position, InertiaMatrix)
.idKey
- The key to identify the payload, not null
nor an empty string. A payload must have been
added using the same key prior to calling this method.mass
- The total mass of the payload attached to the tool output flange of the robot, not null
. Create
it using SimpleValueFactory.createMass(double, Mass.Unit)
.centerOfGravity
- The center of gravity of the payload, not null
. Create it using the
PositionFactory
interface.PayloadNotFoundException
- If no payload exists with the provided idKey
identifier in the current
installation.IllegalMassException
- If the specified mass is not inside the valid range as defined by PolyScope.IllegalCenterOfGravityException
- If any of the values of the specified center of gravity are not inside
the valid range as defined by PolyScope.void updatePayload(String idKey, Mass mass, Position centerOfGravity, InertiaMatrix inertiaMatrix)
idKey
- The key to identify the payload, not null
nor an empty string. A payload must have been
added using the same key prior to calling this method.mass
- The total mass of the payload attached to the tool output flange of the robot, not null
. Create
it using SimpleValueFactory.createMass(double, Mass.Unit)
.centerOfGravity
- The center of gravity of the payload, not null
. Create it using the
PositionFactory
interface.inertiaMatrix
- The inertia matrix of the payload, not null
. Create it using
createInertiaMatrix(double, double, double, double, double, double, MomentOfInertia.Unit)
PayloadNotFoundException
- If no payload exists with the provided idKey
identifier in the current
installation.IllegalMassException
- If the specified mass is not inside the valid range as defined by PolyScope.IllegalCenterOfGravityException
- If any of the values of the specified center of gravity are not inside
the valid range as defined by PolyScope.IllegalInertiaMatrixException
- If any of the values of the specified inertia matrix are not inside the
valid range as defined by PolyScope.void removePayload(String idKey)
idKey
- The identifier key used to add the payload with, not null
nor an empty string.PayloadNotFoundException
- If no payload exists with the provided idKey
identifier in the current
installation.Copyright © 2025. All rights reserved.