@ProviderType
public interface PayloadNodeConfigFactory
This interface can be used to create configurations that can be applied to a Set Payload program node, i.e. a
SetPayloadNode
instance.
Modifier and Type | Method and Description |
---|---|
CustomParametersPayloadNodeConfig |
createCustomParametersConfig(Mass mass,
Position centerOfGravity)
This method creates a configuration for the Set Payload node with custom payload parameters and default value for
the transition time.
|
CustomParametersPayloadNodeConfig |
createCustomParametersConfig(Mass mass,
Position centerOfGravity,
Time transitionTime,
ErrorHandler<Time> transitionTimeErrorHandler)
This method creates a configuration for the Set Payload node with custom payload parameters and specified
transition time.
|
SelectionPayloadNodeConfig |
createSelectionConfig(Payload payload)
This method creates a configuration for the Set Payload node with a pre-selected payload (from the installation)
and with default value for the transition time.
|
SelectionPayloadNodeConfig |
createSelectionConfig(Payload payload,
Time transitionTime,
ErrorHandler<Time> transitionTimeErrorHandler)
This method creates a configuration for the Set Payload node with a pre-selected payload (from the installation)
and specified transition time.
|
SelectionPayloadNodeConfig createSelectionConfig(Payload payload)
This method creates a configuration for the Set Payload node with a pre-selected payload (from the installation) and with default value for the transition time.
Use thePayloadModel
interface to get a list of available payloads from the installation to choose from.payload
- The payload (from the installation) to be selected in the Set Payload node, not null
.SelectionPayloadNodeConfig createSelectionConfig(Payload payload, Time transitionTime, ErrorHandler<Time> transitionTimeErrorHandler)
This method creates a configuration for the Set Payload node with a pre-selected payload (from the installation) and specified transition time.
Use thePayloadModel
interface to get a list of available payloads from the installation to choose from
and use SimpleValueFactory.createTime(double, Time.Unit)
to create the required time parameter.payload
- The payload (from the installation) to be selected in the Set Payload node, not null
.transitionTime
- Transition time is the time it will take to ramp the payload from the actual payload to the
new payload. This can be set to avoid protective stops when handling heavy payloads.
Cannot be null
.transitionTimeErrorHandler
- Error handler for handling validation. If ErrorHandler.AUTO_CORRECT
is
used, this will clamp the specified value to the nearest valid transition time
value.CustomParametersPayloadNodeConfig createCustomParametersConfig(Mass mass, Position centerOfGravity)
This method creates a configuration for the Set Payload node with custom payload parameters and default value for the transition time.
Use SimpleValueFactory.createMass(double, Mass.Unit)
and the PositionFactory
interface to create
the required custom payload parameters.
RobotLimits
interface which can be accessed with RobotModel.getRobotLimits()
(an instance of the
RobotModel
interface can be retrieved through SystemAPI.getRobotModel()
).mass
- The total mass of the payload attached to the tool flange of the robot, not null
. Create it
using SimpleValueFactory.createMass(double, Mass.Unit)
.centerOfGravity
- The center of gravity (CoG), also referred to as center of mass, for the payload. It is
defined as the offset between the center of the tool output flange and the center of gravity
of the attached payload. Cannot be null
. Create it using the PositionFactory
interface.IllegalMassException
- If the specified mass is not inside the valid range as defined by PolyScope.IllegalCenterOfGravityException
- If any of the values of the specified center of gravity are not insideCustomParametersPayloadNodeConfig createCustomParametersConfig(Mass mass, Position centerOfGravity, Time transitionTime, ErrorHandler<Time> transitionTimeErrorHandler)
This method creates a configuration for the Set Payload node with custom payload parameters and specified transition time.
Use SimpleValueFactory.createMass(double, Mass.Unit)
, SimpleValueFactory.createTime(double, Time.Unit)
and the PositionFactory
interface to create the required parameters.
RobotLimits
interface which can be accessed with RobotModel.getRobotLimits()
(an instance of the
RobotModel
interface can be retrieved through SystemAPI.getRobotModel()
).mass
- The total mass of the payload attached to the tool flange of the robot, not null
. Create it
using SimpleValueFactory.createMass(double, Mass.Unit)
.centerOfGravity
- The center of gravity (CoG), also referred to as center of mass, for the payload. It is
defined as the offset between the center of the tool output flange and the center of gravity
of the attached payload. Cannot be null
. Create it using the PositionFactory
interface.transitionTime
- Transition time is the time it will take to ramp the payload from the actual payload to the
new payload. This can be set to avoid protective stops when handling heavy payloads. Cannot
be null
.transitionTimeErrorHandler
- Error handler for handling validation. If ErrorHandler.AUTO_CORRECT
is
used, this will clamp the specified value to the nearest valid transition time
value.IllegalMassException
- If the specified mass is not inside the valid range as defined by PolyScope.IllegalCenterOfGravityException
- If any of the values of the specified center of gravity are not inside
the valid range as defined by PolyScope.Copyright © 2025. All rights reserved.