Class and Description |
---|
SetNodeConfig |
SetNodeConfigFactory
The SetNodeConfigFactory can be used to construct configurations that can be set on a SetNode.
|
Class and Description |
---|
AnalogOutputCurrentSetNodeConfig |
AnalogOutputSelection |
AnalogOutputSelection.SelectionType |
AnalogOutputVoltageSetNodeConfig |
DigitalOutputSelection |
DigitalOutputSelection.SelectionType |
DigitalOutputSetNodeConfig |
ExpressionOutputSelection |
ExpressionOutputSelection.SelectionType |
ExpressionOutputSetNodeConfig |
FloatRegisterOutputSelection |
FloatRegisterOutputSelection.SelectionType |
FloatRegisterOutputSetNodeConfig |
SetNodeConfig |
SetNodeConfig.ConfigType
The configuration type used to determine which type of configuration this instance is.
|
Copyright © 2017. All rights reserved.