Interface | Description |
---|---|
AnalogInput | |
AnalogInputCurrentWaitNodeConfig | |
AnalogInputSelection | |
AnalogInputVoltageWaitNodeConfig | |
AnalogInputWaitNodeConfig | |
DigitalInput | |
DigitalInputSelection | |
DigitalInputWaitNodeConfig | |
ExpressionInputWaitNodeConfig | |
FloatRegisterInput | |
FloatRegisterInputSelection | |
FloatRegisterInputWaitNodeConfig | |
TimeWaitNodeConfig | |
WaitNodeConfig | |
WaitNodeConfigFactory |
The WaitNodeConfigFactory can be used to construct configurations that can be set on a WaitNode.
|
Enum | Description |
---|---|
AnalogInputSelection.SelectionType | |
DigitalInputSelection.SelectionType | |
FloatRegisterInputSelection.SelectionType | |
WaitNodeConfig.ConfigType |
The configuration type used to determine which type of configuration this instance is.
|
Copyright © 2017. All rights reserved.