public static enum Time.Unit extends Enum<Time.Unit>
Enum Constant and Description |
---|
S
Seconds [s] SI unit
|
Modifier and Type | Method and Description |
---|---|
static Time.Unit |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static Time.Unit[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final Time.Unit S
public static Time.Unit[] values()
for (Time.Unit c : Time.Unit.values()) System.out.println(c);
public static Time.Unit valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2017. All rights reserved.