Package | Description |
---|---|
com.ur.urcap.api.domain.value | |
com.ur.urcap.api.domain.value.jointposition | |
com.ur.urcap.api.domain.value.simple |
Modifier and Type | Method and Description |
---|---|
Pose |
PoseFactory.createPose(double x,
double y,
double z,
double rx,
double ry,
double rz,
Length.Unit lengthUnit,
Angle.Unit angleUnit)
Creates a
Pose object for the position and rotation of the robot tool |
boolean |
Pose.epsilonEquals(Pose other,
double lengthEpsilon,
Length.Unit lengthUnit,
double angleEpsilon,
Angle.Unit angleUnit)
Indicates whether of some other Pose is "approximately equal" to this one.
|
boolean |
Rotation.epsilonEquals(Rotation other,
double epsilon,
Angle.Unit unit)
Indicates whether of some other Position is "approximately equal" to this one.
|
double |
Rotation.getRX(Angle.Unit unit)
Provides the rx value in specified units
|
double |
Rotation.getRY(Angle.Unit unit)
Provides the ry value in specified units
|
double |
Rotation.getRZ(Angle.Unit unit)
Provides the rz value in specified units
|
double[] |
Pose.toArray(Length.Unit lengthUnit,
Angle.Unit angleUnit) |
Modifier and Type | Method and Description |
---|---|
JointPositions |
JointPositionFactory.createJointPositions(double base,
double shoulder,
double elbow,
double wrist1,
double wrist2,
double wrist3,
Angle.Unit unit)
Creates a
JointPositions object for six revolute joints using the provided angles and unit type |
boolean |
JointPosition.epsilonEquals(JointPosition other,
double epsilon,
Angle.Unit unit)
Indicates whether some other JointPosition is "approximately equal" to this one.
|
boolean |
JointPositions.epsilonEquals(JointPositions other,
double epsilon,
Angle.Unit unit)
Indicates whether each element of some other JointPositions is "approximately equal in tolerance" to this one.
|
double |
JointPosition.getAngle(Angle.Unit unit)
Provides the angle offset in the range [0:2pi[ (RAD) or [0:360[ (DEG)
|
double |
JointPosition.getPosition(Angle.Unit unit)
Provides the position value including all revolutions in the specified unit
|
Modifier and Type | Method and Description |
---|---|
static Angle.Unit |
Angle.Unit.valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static Angle.Unit[] |
Angle.Unit.values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
Modifier and Type | Method and Description |
---|---|
Angle |
SimpleValueFactory.createAngle(double value,
Angle.Unit unit) |
double |
Angle.getAs(Angle.Unit unit)
Provides the value in specified units
|
Copyright © 2017. All rights reserved.