public interface Variable
Modifier and Type | Interface and Description |
---|---|
static class |
Variable.Type
The variable type used to determine which type of variable this instance is.
|
Modifier and Type | Method and Description |
---|---|
boolean |
equals(Object object) |
String |
getDisplayName()
Note: The variable can be renamed at any time
|
Variable.Type |
getType() |
int |
hashCode() |
String |
toString() |
Variable.Type getType()
String getDisplayName()
boolean equals(Object object)
int hashCode()
Copyright © 2017. All rights reserved.