Class and Description |
---|
UntilNodeConfig |
UntilNodeConfigFactory |
Class and Description |
---|
BlendParameters |
BlendParameters.ParameterType
Blend Parameters can be of different types
The parameter type is used to determine the explicit blend parameters (can be used in place of instanceof operations)
|
CustomDecelerationParameters |
CustomDecelerationParameters.Type |
DecelerationParameters |
DecelerationParameters.ParameterType
The deceleration parameter type used to determine which type of deceleration parameter this instance is.
|
DistanceUntilNodeConfig |
ExpressionUntilNodeConfig |
ReachedWaypointUntilNodeConfig |
UntilNodeConfig |
UntilNodeConfig.ConfigType
The configuration type used to determine which type of configuration this instance is.
|
Copyright © 2019. All rights reserved.