Class and Description |
---|
WaitNodeConfig |
WaitNodeConfigFactory
The WaitNodeConfigFactory can be used to construct configurations that can be set on a WaitNode.
|
Class and Description |
---|
AnalogInputCurrentWaitNodeConfig |
AnalogInputSelection |
AnalogInputSelection.SelectionType |
AnalogInputVoltageWaitNodeConfig |
AnalogInputWaitNodeConfig |
DigitalInputSelection |
DigitalInputSelection.SelectionType |
DigitalInputWaitNodeConfig |
ExpressionInputWaitNodeConfig |
FloatRegisterInputSelection |
FloatRegisterInputSelection.SelectionType |
FloatRegisterInputWaitNodeConfig |
TimeWaitNodeConfig |
WaitNodeConfig |
WaitNodeConfig.ConfigType
The configuration type used to determine which type of configuration this instance is.
|
Copyright © 2019. All rights reserved.