@ProviderType public interface MultiGripperSupport extends CapabilitySupport
 This interface represents the support for multiple grippers provided by a multi-gripper device (a GripperDevice
 instance), i.e. a gripper device supporting the multi-gripper capability.
 
 The interface provides information which can be used to configure the multi-gripper capability of a multi-gripper
 device used by a GripperNode. This includes access to the set of individual grippers (available in the
 multi-gripper device) which allows for selecting a specific gripper when creating a GripperNode
 configuration.
 
 An instance of this interface can be acquired by calling the GripperDevice.getCapabilitySupport(Class) with
 the class of the MultiGripperSupport interface as argument. The returned MultiGripperSupport instance
 is wrapped in an Optional. Always use Optional.isPresent() to check if a specific gripper device is
 a multi-gripper (i.e. supports the multi-gripper capability) before accessing it using Optional.get().
 
| Modifier and Type | Method and Description | 
|---|---|
List<SelectableGripper> | 
getSelectableGrippers()
 Get the set of individual grippers available in the multi-gripper device. 
 | 
List<SelectableGripper> getSelectableGrippers()
Get the set of individual grippers available in the multi-gripper device. Note that this list of individual grippers is only applicable for a specific multi-gripper device.
 The returned list can be used to select a gripper when creating a configuration for a GripperNode with
 the GripActionConfigBuilder or ReleaseActionConfigBuilder interface.
 
GripperNode.Copyright © 2023. All rights reserved.