public interface FeatureContributionModel
This interface provides functionality for adding, updating and removing features in PolyScope.
Note: This interface must only be used in an installation contribution.| Modifier and Type | Method and Description |
|---|---|
Feature |
addFeature(String idKey,
String suggestedName,
Pose pose)
Add a feature to the current PolyScope installation.
|
Feature |
getFeature(String idKey)
Returns the feature previously added by this URCap using the same
idKey identifier. |
void |
removeFeature(String idKey)
Remove a feature added by this URCap from PolyScope.
|
void |
updateFeature(String idKey,
Pose newPose)
Update the pose of an existing feature added by this URCap.
|
Feature addFeature(String idKey, String suggestedName, Pose pose)
Add a feature to the current PolyScope installation.
This makes the feature selectable by the end user as well as available to other URCap contributions (through theFeatureModel interface). The feature is not modifiable by the end user or other URCaps.idKey - The key to identify this feature by, not null nor an empty string. The key is for this URCap
only, i.e. it only has to be unique for this URCap and not "globally" for other URCaps.suggestedName - Suggested name for the feature, not null nor an empty string. Valid names must match
regex [a-zA-Z][a-zA-Z0-9_]{0,14} for a total of 15 characters. The final name can be retrieved
from the returned feature instance.pose - The pose of the feature with respect to the robot base, not null.FeatureAlreadyAddedException - If a feature has previously been added using the same idKey identifier.
Use getFeature(String) to check if the feature has already been added
to the current installation.
Use updateFeature(String, Pose) to update the feature.IllegalFeatureNameException - If the suggested name does not match required regex.Feature getFeature(String idKey)
idKey identifier. Use this to verify if
the feature is present in the current installation.idKey - The key to identify this feature by, not null nor an empty string.null if no feature exists in the current installation (with the specified idKey
identifier).void updateFeature(String idKey, Pose newPose)
idKey - The key to identify the feature, not null nor an empty string. A feature must have been added
using the same key prior to calling this method.newPose - The new pose to set for the feature with respect to the robot base, not null.FeatureNotFoundException - If no feature exists with the provided idKey identifier in the current
installation.void removeFeature(String idKey)
idKey - The identifier key used to add the feature with, not null nor an empty string.FeatureNotFoundException - If no feature exists with the provided idKey identifier in the current
installation.Copyright © 2023. All rights reserved.