public interface WaitNode extends ProgramNode
Modifier and Type | Method and Description |
---|---|
WaitNodeConfig |
getConfig() |
WaitNodeConfigFactory |
getConfigFactory() |
WaitNode |
setConfig(WaitNodeConfig config)
Set a configuration on this node.
|
WaitNodeConfigFactory getConfigFactory()
WaitNode setConfig(WaitNodeConfig config)
config
- the configuration to be set.InvalidDomainException
- if config is analog input using voltage and the IO is configured to current
or vice versa.IllegalStateException
- if called from a Swing-based URCap outside of an UndoableChanges
scope (see also UndoRedoManager
).WaitNodeConfig getConfig()
Copyright © 2023. All rights reserved.