public interface DirectionNodeConfigBuilder
DirectionNodeConfigBuilder
instance.
For any configuration parameter where a value is not specified (using the corresponding set method), a default value
will be used when the new configuration is built whereas the original value will be used when an existing configuration
was copied using the copyFrom(DirectionNodeConfig)
method.
DirectionNodeConfig newConfig = configBuilder.setFeature(feature)
.setDirection(DirectionAxis.X_PLUS)
.build();
To change the feature selection in the current configuration, use the following code snippet to build a new updated
configuration:
configBuilder.copyFrom(currentConfig);
DirectionNodeConfig updatedConfig = configBuilder.setFeature(feature)
.build();
Modifier and Type | Method and Description |
---|---|
DirectionNodeConfig |
build()
Build the configuration for a Direction node.
|
DirectionNodeConfigBuilder |
copyFrom(DirectionNodeConfig source)
Copy values from one configuration (source) to another (this) builder.
|
DirectionNodeConfigBuilder |
setDirection(DirectionAxis.Axis axis)
Sets the direction for a Direction node.
|
DirectionNodeConfigBuilder |
setDirection(Expression expression)
Sets the direction for a Direction node.
|
DirectionNodeConfigBuilder |
setFeature(Feature feature)
Set feature for a Direction node.
|
DirectionNodeConfigBuilder |
setSharedFeature()
Sets shared feature for a Direction node.
|
DirectionNodeConfigBuilder |
setSharedToolMotionParameters()
Sets shared tool motion parameters for a Direction node.
|
DirectionNodeConfigBuilder |
setToolMotionParameters(Speed toolSpeed,
ErrorHandler<Speed> toolSpeedErrorHandler,
Acceleration toolAcceleration,
ErrorHandler<Acceleration> toolAccelerationErrorHandler)
Sets tool motion parameters for a Direction node.
|
DirectionNodeConfigBuilder copyFrom(DirectionNodeConfig source)
source
- the original configuration to copy values from.DirectionNodeConfigBuilder setSharedToolMotionParameters()
DirectionNodeConfigBuilder setToolMotionParameters(Speed toolSpeed, ErrorHandler<Speed> toolSpeedErrorHandler, Acceleration toolAcceleration, ErrorHandler<Acceleration> toolAccelerationErrorHandler)
toolSpeed
- the tool speed to be achieved, not null
.toolSpeedErrorHandler
- error handler for handling validation. If using ErrorHandler.AUTO_CORRECT
this will clamp the value to the nearest valid tool speed value.toolAcceleration
- the tool acceleration to be used for the movement, not null
.toolAccelerationErrorHandler
- error handler for handling validation. If using ErrorHandler.AUTO_CORRECT
this will clamp the value to the nearest valid tool acceleration value.DirectionNodeConfigBuilder setFeature(Feature feature)
feature
- the feature for a direction node, not null
.DirectionNodeConfigBuilder setSharedFeature()
DirectionNodeConfigBuilder setDirection(Expression expression)
expression
- any expression that resolves to a vector (e.g. '[1.0, 0.0, 0.0]').DirectionNodeConfigBuilder setDirection(DirectionAxis.Axis axis)
axis
- linear axis to move along.DirectionNodeConfig build()
Build the configuration for a Direction node.
A default configuration can be built by calling this method without invoking any of the set methods in this interface.Copyright © 2023. All rights reserved.