Interface | Description |
---|---|
CustomParametersPayloadNodeConfig |
This interface represents a configuration of the Set Payload node which is using custom payload parameters.
|
PayloadNodeConfig |
This base interface represents a configuration of the Set Payload program node, i.e.
|
PayloadNodeConfigFactory |
This interface can be used to create configurations that can be applied to a Set Payload program node, i.e.
|
SelectionPayloadNodeConfig |
This interface represents a configuration of the Set Payload node where a payload (from the installation) has been
selected.
|
Enum | Description |
---|---|
PayloadNodeConfig.ConfigType |
The configuration type used to determine which type of configuration this instance is.
|
Copyright © 2023. All rights reserved.