Interface | Description |
---|---|
AnalogOutput | |
AnalogOutputCurrentSetNodeConfig | |
AnalogOutputSelection | |
AnalogOutputVoltageSetNodeConfig | |
DigitalOutput | |
DigitalOutputSelection | |
DigitalOutputSetNodeConfig | |
ExpressionOutput | |
ExpressionOutputSelection | |
ExpressionOutputSetNodeConfig | |
FloatRegisterOutput | |
FloatRegisterOutputSelection | |
FloatRegisterOutputSetNodeConfig | |
SetNodeConfig | |
SetNodeConfigFactory |
This interface can be used to construct configurations that can be set on a SetNode.
|
SingleDigitalPulseSetNodeConfig |
Enum | Description |
---|---|
AnalogOutputSelection.SelectionType | |
DigitalOutputSelection.SelectionType | |
ExpressionOutputSelection.SelectionType | |
FloatRegisterOutputSelection.SelectionType | |
SetNodeConfig.ConfigType |
The configuration type used to determine which type of configuration this instance is.
|
Copyright © 2023. All rights reserved.