Interface | Description |
---|---|
MoveJConfigBuilder |
This interface can be used to build a single MoveJ configuration that can be applied to a Move node.
|
MoveLConfigBuilder |
This interface can be used to build a single MoveL configuration that can be applied to a Move node.
|
MoveNodeConfigBuilders |
This interface provides access to a set of builders which can be used to create Move node configurations
for all the different supported move types.
|
MovePConfigBuilder |
This interface can be used to build a single MoveP configuration that can be applied to a Move node.
|
Copyright © 2023. All rights reserved.