Interface | Description |
---|---|
FeatureSelection | |
MoveJMotionParameters | |
MoveJMoveNodeConfig | |
MoveLMotionParameters | |
MoveLMoveNodeConfig | |
MoveNodeConfig | |
MoveNodeConfigFactory | Deprecated
Use the configuration builders available in
MoveNodeConfigBuilders interface which is accessible
through MoveNode.getConfigBuilders() . |
MoveNodeFeature | |
MoveNodeTCP | |
MovePMotionParameters | |
MovePMoveNodeConfig | |
TCPSelection | |
TCPSelectionFactory |
This interface supplies methods for creating TCP selections for a Move node configuration.
|
Enum | Description |
---|---|
FeatureSelection.SelectionType | |
MoveNodeConfig.ConfigType |
The configuration type used to determine which type of configuration this instance is.
|
TCPSelection.SelectionType |
Copyright © 2023. All rights reserved.