Modifier and Type | Method and Description |
---|---|
void |
TCPConfiguration.setTCP(String suggestedName,
Pose tcpPose)
Add a TCP for the device to PolyScope.
|
void |
TCPConfiguration.updateTCP(Pose tcpPose)
Update the offset of the device's TCP.
|
Modifier and Type | Method and Description |
---|---|
Pose |
DataModel.get(String key,
Pose defaultValue)
Get the
Pose value assigned to the specified key. |
Modifier and Type | Method and Description |
---|---|
Pose |
DataModel.get(String key,
Pose defaultValue)
Get the
Pose value assigned to the specified key. |
void |
DataModel.set(String key,
Pose value)
Assign a
Pose value to the specified key. |
Modifier and Type | Method and Description |
---|---|
Pose |
Feature.getPose()
Returns the Cartesian location of the feature
|
Modifier and Type | Method and Description |
---|---|
Feature |
FeatureContributionModel.addFeature(String idKey,
String suggestedName,
Pose pose)
Add a feature to the current PolyScope installation.
|
void |
FeatureContributionModel.updateFeature(String idKey,
Pose newPose)
Update the pose of an existing feature added by this URCap.
|
Modifier and Type | Method and Description |
---|---|
Pose |
FixedPositionDefinedWaypointNodeConfig.getPose()
This method returns the pose for the Cartesian location of the Waypoint node, i.e.
|
Modifier and Type | Method and Description |
---|---|
FixedPositionDefinedWaypointNodeConfig |
WaypointNodeConfigFactory.createFixedPositionConfig(Pose poseIncludingTcp,
JointPositions qNear,
BlendParameters blendParameters,
WaypointMotionParameters waypointMotionParameters)
|
FixedPositionDefinedWaypointNodeConfig |
WaypointNodeConfigFactory.createFixedPositionConfig(Pose poseIncludingTcp,
JointPositions qNear,
Pose tcpOffset,
BlendParameters blendParameters,
WaypointMotionParameters waypointMotionParameters)
Creates a fixed position configuration for a waypoint with a defined pose.
|
Modifier and Type | Method and Description |
---|---|
Pose |
TCP.getOffset() |
Modifier and Type | Method and Description |
---|---|
TCP |
TCPContributionModel.addTCP(String idKey,
String suggestedName,
Pose offset)
Add a TCP to the current PolyScope installation.
|
void |
TCPContributionModel.updateTCP(String idKey,
Pose newOffset)
Update the offset of an existing TCP added by this URCap.
|
Modifier and Type | Method and Description |
---|---|
abstract void |
RobotPositionCallback.onOk(Pose pose,
JointPositions q)
Deprecated.
This method is called if the end user accepts the robot position.
|
Modifier and Type | Method and Description |
---|---|
PoseMovementConfiguration |
RobotMovement.createPoseMovementConfiguration(Pose pose)
Create a robot movement configuration object to be used for robot movement.
|
void |
RobotMovement.requestUserToMoveRobot(Pose pose,
RobotMovementCallback callback)
Transition to the Automove screen to allow/request the end user to move the robot (either automatically or manually)
to a desired target position specified by a pose.
|
Modifier and Type | Method and Description |
---|---|
Pose |
PoseFactory.createPose(double x,
double y,
double z,
double rx,
double ry,
double rz,
Length.Unit lengthUnit,
Angle.Unit angleUnit)
Creates an object representing a pose with the specified Cartesian position and orientation (rotation)
|
Pose |
PoseFactory.createPose(Position position,
Rotation rotation)
Creates an object representing a pose with the specified Cartesian position and orientation (rotation).
|
Modifier and Type | Method and Description |
---|---|
boolean |
Pose.epsilonEquals(Pose other,
double epsilon)
Deprecated.
|
boolean |
Pose.epsilonEquals(Pose other,
double positionEpsilon,
Length.Unit lengthUnit,
double rotationEpsilon,
Angle.Unit angleUnit)
Indicates whether some other
Pose is "approximately equal" to this one. |
Modifier and Type | Method and Description |
---|---|
Pose |
PositionParameters.getPose() |
Pose |
PositionParameters.getTCPOffset() |
Copyright © 2025. All rights reserved.