Class and Description |
---|
ScrewdriverCapabilities
Register the capabilities of the screwdriver using this interface.
|
ScrewdriverFeedbackCapabilities
Register the feedback capabilities of the screwdriver using this interface.
|
Class and Description |
---|
DriveScrewNotOKParameters
This interface provides parameters relevant for generating script code for the Drive Screw Not OK feedback capability
(registered using
ScrewdriverFeedbackCapabilities.registerDriveScrewNotOKCapability(ScriptCodeGenerator) ). |
DriveScrewOKParameters
This interface provides parameters relevant for generating script code for the Drive Screw OK feedback capability
(registered using
ScrewdriverFeedbackCapabilities.registerDriveScrewOKCapability(ScriptCodeGenerator) ). |
FeedScrewParameters
This interface provides parameters relevant for generating script code for the Feed Screw capability
(registered using
ScrewdriverCapabilities.registerFeedScrewCapability(ScriptCodeGenerator) ). |
PrepareToStartScrewdriverParameters
This interface provides parameters relevant for generating script code for the Prepare To Start Screwdriver capability
(registered using
ScrewdriverCapabilities.registerPrepareToStartScrewdriverCapability(ScriptCodeGenerator) ). |
ProgramSelectionParameters
This interface provides parameters relevant for generating script code for the Program Selection capability
(registered using
ScrewdriverCapabilities.registerProgramSelectionCapability(ScrewdriverProgramListProvider, ScriptCodeGenerator) ). |
ScrewdriverReadyParameters
This interface provides the parameters relevant for generating script for the Screwdriver Ready feedback operation
capability (registered using
ScrewdriverFeedbackCapabilities.registerScrewdriverReadyCapability(ScriptCodeGenerator) ). |
Copyright © 2023. All rights reserved.