Modifier and Type | Method and Description |
---|---|
boolean |
CapabilityManager.hasCapability(Capability capability)
Verify availability of a capability on the robot/system.
|
Modifier and Type | Class and Description |
---|---|
class |
ProgramNodeCapability
This
enum contains capabilities of the built-in PolyScope program nodes that may or may not be available on
the underlying robot/system. |
Modifier and Type | Class and Description |
---|---|
class |
ToolIOCapability
This
enum contains capabilities of the Tool I/O Interface that may or may not be available on the underlying
robot/system. |
Copyright © 2023. All rights reserved.