Interface | Description |
---|---|
CustomPayloadParameters |
This interface represents a configuration of the payload setting for a Gripper node where custom payload parameters
are used.
|
GripActionConfig |
This interface represents a Gripper node configuration for a grip action.
|
GripActionConfigBuilder |
This interface can be used to build a single gripper configuration for a grip action.
|
GripperNodeConfig |
This base interface represents a configuration of a Gripper program node (i.e.
|
PayloadSelection |
This interface represents a configuration of the payload setting for a Gripper node where a payload (from the
installation) has been selected.
|
PayloadSetting |
This interface represents the configuration of the payload setting for a gripper node.
|
ReleaseActionConfig |
This interface represents a Gripper node configuration for a release action.
|
ReleaseActionConfigBuilder |
This interface can be used to build a single gripper configuration for a release action.
|
SelectableGripper |
This interface represents an individual gripper in a multi-gripper device, i.e.
|
UndefinedActionConfig |
This interface represents a Gripper node configuration where the gripper action (i.e.
|
Enum | Description |
---|---|
GripperNodeConfig.ConfigType |
The configuration type used to determine which type of configuration this instance is.
|
PayloadSetting.SettingType |
The setting type used to determine which type of setting this instance is.
|
Copyright © 2023. All rights reserved.